FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Updating to the 64-bit Windows 7 version of GX Works2
FAQ
Updating to the 64-bit Windows 7 version of GX Works2
The update file for GX Works2 is being executed on a 64-bit Windows 7-based personal computer with the GX Works2 CD placed in the drive.
The update file asks the location of the CD during execution.
When the location of the CD is specified, a message saying it does not support the 64-bit version is displayed.
Can I install the file in this condition?
The update file asks the location of the CD during execution.
When the location of the CD is specified, a message saying it does not support the 64-bit version is displayed.
Can I install the file in this condition?
- Category :
Answer
The message is displayed because the version of the CD does not support the 64-bit version.
Execute the installation procedure in the condition.
Execute the installation procedure in the condition.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)