FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > CPU modules supporting the serial communication function
FAQ
CPU modules supporting the serial communication function
Which CPU modules can be communicated via RS-232 interface using the serial communication function from a personal computer,
an Human Machine Interface (HMI), etc.?
an Human Machine Interface (HMI), etc.?
- Category :
Answer
CPU modules supporting the serial communication function are as follows.
- Q00UJCPU,Q00UCPU,Q01UCPU
- Q02UCPU 10102 or later (with GX Works2 1.15R or later or GX Developer 8.76E or later)
- Q03UDCPU, Q04UDHCPU, Q06UDHCPU, Q10UDHCPU, Q13UDHCPU, Q20UDHCPU, Q26UDHCPU 13062 or later
(with GX Works2 1.62Q or later)
- Q00UJCPU,Q00UCPU,Q01UCPU
- Q02UCPU 10102 or later (with GX Works2 1.15R or later or GX Developer 8.76E or later)
- Q03UDCPU, Q04UDHCPU, Q06UDHCPU, Q10UDHCPU, Q13UDHCPU, Q20UDHCPU, Q26UDHCPU 13062 or later
(with GX Works2 1.62Q or later)
- Product Name
- MELSEC-Q Series
- Series
- CPU