FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Unable to select [Transfer Setup]
FAQ
Unable to select [Transfer Setup]
[Transfer Setup] on the menu is grayed out and the connection destination cannot be changed.
How can I enable the grayed out item?
How can I enable the grayed out item?
- Category :
Answer
If a circuit is being monitored or a monitor window such as the device batch monitor window is open,
[Transfer Setup] on the menu is grayed out.
Select [Window] on the menu and check currently opened windows.
Stopping monitoring the circuit or closing the monitor window enables [Transfer Setup] on the menu.
[Transfer Setup] on the menu is grayed out.
Select [Window] on the menu and check currently opened windows.
Stopping monitoring the circuit or closing the monitor window enables [Transfer Setup] on the menu.
- Product Name
- MELSEC-Q Series
- Series
- Software Package (GPP function)