FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Boot operation from the standard ROM
FAQ
Boot operation from the standard ROM
Is the boot operation of universal model QCPU from the standard ROM possible?
- Category :
Answer
The boot operation from the standard ROM is not possible.
The program memory of universal model QCPU is a flash ROM.
Thus, writing in the program memory achieves a ROM operation.
The program memory of universal model QCPU is a flash ROM.
Thus, writing in the program memory achieves a ROM operation.
- Product Name
- MELSEC-Q Series
- Series
- CPU