FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > How to turn OFF the "COM.ERR" LED of the Ethernet module
FAQ
How to turn OFF the "COM.ERR" LED of the Ethernet module
Is it possible to turn OFF the "COM.ERR" LED of an Ethernet module installed to the standby system of a redundant system?
- Category :
Answer
The LED can be turned OFF by operations from GX Developer. The operation method is as follows.
(1) Connect to the CPU in the standby system in Transfer Setup.
- Connect to the CPU in the standby system with "No specified system" selected.
(2) Turn off the "COM.ERR" LED.
- Click the "COM.ERR off" button in Ethernet diagnostics dialog box.
(1) Connect to the CPU in the standby system in Transfer Setup.
- Connect to the CPU in the standby system with "No specified system" selected.
(2) Turn off the "COM.ERR" LED.
- Click the "COM.ERR off" button in Ethernet diagnostics dialog box.
- Product Name
- MELSEC-Q Series
- Series
- CPU