FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Resolution provided for Q64AD/Q68ADV/Q68ADI
FAQ
Resolution provided for Q64AD/Q68ADV/Q68ADI
Does the resolution provided for Q64AD/Q68ADV/Q68ADI become higher if the analog input range is set to "User range setting" and the analog input value corresponding to the maximum digital output value is set to a smaller value using the gain setting?
- Category :
Answer
The maximum resolution for the user range setting does not change.


- Product Name
- MELSEC-Q Series
- Series
- A / D Conversion Module