FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Life expectancy of the CompactFlash card used in the high speed data logger module
FAQ
Life expectancy of the CompactFlash card used in the high speed data logger module
What is the life expectancy of the CompactFlash card used in the high speed data logger module?
- Category :
Answer
The life expectancy is determined by the following calculation.
Life expectancy (year) = Total writable size (GB) / 1 year write size (GB/year)
For more details of the calculation, refer to the following manual.
- "High Speed Data Logger Module User's Manual" Section 15.7
Life expectancy (year) = Total writable size (GB) / 1 year write size (GB/year)
For more details of the calculation, refer to the following manual.
- "High Speed Data Logger Module User's Manual" Section 15.7
- Product Name
- MELSEC-Q Series
- Series
- Other Modules (terminal block, connector, cable etc.)