FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Label programs in GX Works2
FAQ
Label programs in GX Works2
Can a label program be changed to an unlabeled program in GX Works2?
- Category :
Answer
Change the program using the following method.
Write the label program to the programmable controller CPU and perform PLC read for the parameters and the program without selecting symbolic information in the Read from PLC window.
Write the label program to the programmable controller CPU and perform PLC read for the parameters and the program without selecting symbolic information in the Read from PLC window.
- Product Name
- MELSEC-Q Series
- Series
- Software Package (GPP function)