FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Settings of the built-in Ethernet port of the universal model QCPU
FAQ
Settings of the built-in Ethernet port of the universal model QCPU
Where can I make settings of the built-in Ethernet port of a universal model QCPU?
- Category :
Answer
Make settings of the built-in Ethernet port in the [Built-in Ethernet Port Setting] tab of the PLC parameter
in GX Works2 or GX Developer.
in GX Works2 or GX Developer.
- Product Name
- MELSEC-Q Series
- Series
- CPU