FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Memory allocation for online change in GX Works2
FAQ
Memory allocation for online change in GX Works2
What is the maximum number of steps that can be set for "Allocate Memory for 'Online Change'" in GX Works2?
- Category :
Answer
The capacity of parameters and programs subtracted from the program capacity for the CPU type in use equals the size of the maximum number of steps.
- Product Name
- MELSEC-Q Series
- Series
- Software Package (GPP function)