FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Setting of "Target MODBUS(R) device head number"
FAQ
Setting of "Target MODBUS(R) device head number"
What do I set for the Automatic communication parameter "Target MODBUS(R) device head number" of the MODBUS(R) interface module QJ71MB91/QJ71MT91?
- Category :
Answer
Set "(Last five digits of actual device number) - 1" for the Target MODBUS(R) device head number.
Example) For the holding register 400018, set "17".
Example) For the holding register 400018, set "17".
- Product Name
- MELSEC-Q Series
- Series
- MODBUS