FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Update timing of QD75 current feed value and machine feed value
FAQ
Update timing of QD75 current feed value and machine feed value
When are the current feed value and the machine feed value of QD75P1/P2/P4/D1/D2/D4 updated?
- Category :
Answer
The values are updated at the timing described below.
- Current feed value: 1.8 ms
- Machine feed value: 56.8 ms
- Current feed value: 1.8 ms
- Machine feed value: 56.8 ms
- Product Name
- MELSEC-Q Series
- Series
- Positioning Module