FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Remedy for the division-related operation error
FAQ
Remedy for the division-related operation error
An operation error occurs when a division operation is performed. What is the remedy for the error?
- Category :
Answer
The operation error occurs when the divisor is 0.
Create a program in which a comparison operation instruction or another method executes a division instruction only when the divider is not 0 .
Create a program in which a comparison operation instruction or another method executes a division instruction only when the divider is not 0 .
- Product Name
- MELSEC-Q Series
- Series
- CPU