FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > SD memory cards used for Q24DHCCPU-V
FAQ
SD memory cards used for Q24DHCCPU-V
Which SD memory cards does Q24DHCCPU-V support?
- Category :
Answer
Mitsubishi Electric's SD memory cards, which can be installed into Q24DHCCPU-V, are shown below.
- NZ1MEM-2GBSD (memory capacity: 2Gbytes)
- NZ1MEM-2GBSD (memory capacity: 2Gbytes)
- NZ1MEM-4GBSD (memory capacity: 4Gbytes)
- NZ1MEM-8GBSD (memory capacity: 8Gbytes)
- NZ1MEM-16GBSD (memory capacity: 16Gbytes)
- L1MEM-2GBSD (memory capacity: 2Gbytes) (Discontinued production in July 2015)
- L1MEM-4GBSD (memory capacity: 4Gbytes) (Discontinued production in July 2015)
For installable non-Mitsubishi products, refer to the following technical bulletin.
- C Controller module applicable product information
- NZ1MEM-16GBSD (memory capacity: 16Gbytes)
- L1MEM-2GBSD (memory capacity: 2Gbytes) (Discontinued production in July 2015)
- L1MEM-4GBSD (memory capacity: 4Gbytes) (Discontinued production in July 2015)
For installable non-Mitsubishi products, refer to the following technical bulletin.
- C Controller module applicable product information
- Product Name
- MELSEC-Q Series
- Series
- C Language Controller