FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU
FAQ
Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU
Can I use an A-compatible 1E frame of the MC protocol for the built-in Ethernet port in the L series CPU?
- Category :
Answer
The built-in Ethernet port in the L series is compatible only with a QnA-compatible 3E frame of the MC protocol. An A-compatible 1E frame is not supported.
- Product Name
- MELSEC-L Series
- Series
- L Series