FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Communication data code of the MC protocol for the built-in Ethernet port in LCPU
FAQ
Communication data code of the MC protocol for the built-in Ethernet port in LCPU
Regarding the communication data code of the MC protocol for the built-in Ethernet port in the L series CPU, is it binary code communication, or ASCII code communication?
- Category :
Answer
The communication data code is selectable by the communication data code setting in
[Parameter] -> [PLC Parameter] -> [Built-in Ethernet Port Setting].
[Parameter] -> [PLC Parameter] -> [Built-in Ethernet Port Setting].
- Product Name
- MELSEC-L Series
- Series
- L Series