FAQ


FAQAbout Products
 
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Simple PLC communication function
FAQ
Simple PLC communication function
      What is the simple PLC communication function?
    
  - Category :
Answer
    This function allows data communications between specified devices at the specified timing, using the built-in Ethernet. 
Device data such as production data can be transferred without a program just by doing simple settings from a programming too.
Furthermore, this function allows for easy communication not only between the L series devices, but also with existing systems that use the Q series and QnA/A series. The target modules are CPU modules whose first 5 digits of the serial number are "13042" or later.
    Device data such as production data can be transferred without a program just by doing simple settings from a programming too.
Furthermore, this function allows for easy communication not only between the L series devices, but also with existing systems that use the Q series and QnA/A series. The target modules are CPU modules whose first 5 digits of the serial number are "13042" or later.
- Product Name
- MELSEC-L Series
- Series
- CPU