FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Method to prevent the BAT.LED from turning on
FAQ
Method to prevent the BAT.LED from turning on
Is there any method to prevent the BAT.LED from turning on when LCPU is running without the battery installed?
- Category :
Answer
To prevent an LED from turning on when an error occurs, set 0 to the relevant factor number setting area (4 bits for each) in SD207 to SD209.
To disable the BAT.LED indication for battery errors, write a hexadecimal "00A0" to SD209. (The priority order of battery error is 9.)
To disable the BAT.LED indication for battery errors, write a hexadecimal "00A0" to SD209. (The priority order of battery error is 9.)
- Product Name
- MELSEC-L Series
- Series
- CPU