FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > PLC write not possible due to memory overload
FAQ
PLC write not possible due to memory overload
When I tried to write a comment to the program memory in LCPU, it failed due to memory overload. What is the remedy?
- Category :
Answer
If comments cannot be stored in the program memory, write them in the standard ROM or a memory card.
Calculate the memory capacity in GX Works2 or GX Developer before performing PLC write to check whether it is possible to write all data to the program memory.
Calculate the memory capacity in GX Works2 or GX Developer before performing PLC write to check whether it is possible to write all data to the program memory.
- Product Name
- MELSEC-L Series
- Series
- CPU