FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Cable length to connect to built-in Ethernet port in LCPU
FAQ
Cable length to connect to built-in Ethernet port in LCPU
When a hub is used, what is the max. cable length connectable with the built-in Ethernet port in the L series CPU?
- Category :
Answer
The maximum length between a hub and a node is 100 m. The max. length connectable to a hub is 200m.
When repeater hubs are used in cascade connection, the maximum length between hubs is 5 m for 100BASE-TX, and 100 m for 10BASE-T. When switching hubs are used, verify with the manufacturer.
When repeater hubs are used in cascade connection, the maximum length between hubs is 5 m for 100BASE-TX, and 100 m for 10BASE-T. When switching hubs are used, verify with the manufacturer.
- Product Name
- MELSEC-L Series
- Series
- L Series