FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Simultaneous broadcast transmission setting for built-in Ethernet port LCPU
FAQ
Simultaneous broadcast transmission setting for built-in Ethernet port LCPU
How do I configure the setting to send simultaneous broadcasts during socket communication of L series CPU with built-in Ethernet port?
- Category :
Answer
To send simultaneous broadcast using UDP, set the parameters as follows.
- Destination IP Address: FF.FF.FF.FFh
- Destination Port Number: Other than FFFFh (Specify the port number dedicated to simultaneous broadcast)
- Destination IP Address: FF.FF.FF.FFh
- Destination Port Number: Other than FFFFh (Specify the port number dedicated to simultaneous broadcast)
- Product Name
- MELSEC-L Series
- Series
- L Series