FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > SD1286 of LCPU with built-in Ethernet port
FAQ
SD1286 of LCPU with built-in Ethernet port
During socket communication of L series CPU with built-in Ethernet port, how does the special register SD1286 (Receive state signal) correspond to the connection number?
- Category :
Answer
The bits 0 to F of the special register SD1286 (Receive state signal) correspond to the connection numbers 1 to 16. When it receives data, the corresponding bit will turn ON.
- Product Name
- MELSEC-L Series
- Series
- L Series