FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Causes to why SD1286 does not turn on during socket communication of LCPU
FAQ
Causes to why SD1286 does not turn on during socket communication of LCPU
SD1286 (Receive state signal) does not turn on during socket communication of L series CPU. What are the possible causes?
- Category :
Answer
Check the following.
- Whether the external device specifies the port number of the corresponding connection to the L series CPU.
- In the TCP fixed-length receive mode, whether the size of the data sent by the external device is the same as
the specified receive data size.
- Whether the external device specifies the port number of the corresponding connection to the L series CPU.
- In the TCP fixed-length receive mode, whether the size of the data sent by the external device is the same as
the specified receive data size.
- Product Name
- MELSEC-L Series
- Series
- L Series