FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > How to use LCPU connector terminals
FAQ
How to use LCPU connector terminals
How do I use the LCPU connector terminals (A01 to A20 and B01 to B20)?
- Category :
Answer
The LCPU connector terminals can be used as terminals for built-in I/O function. The setting of the built-in I/O function can be configured with the parameters of the programming tool.
For more details, refer to "MELSEC-L CPU Module User's Manual (Built-In I/O Function)".
For more details, refer to "MELSEC-L CPU Module User's Manual (Built-In I/O Function)".
- Product Name
- MELSEC-L Series
- Series
- CPU