FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Error code "2401" in LCPU
FAQ
Error code "2401" in LCPU
The error code "2401" is displayed on LCPU.
The individual information parameter number is "1100H". Are there any remedies?
The individual information parameter number is "1100H". Are there any remedies?
- Category :
Answer
The error code "2401" is "FILE SET ERROR".
The individual information parameter number "1100H" corresponds to a file register.
The cause of the error is that the file register file specified by the parameter cannot be created.
Check the amount of free space of the memory in which the file register file is created.
The individual information parameter number "1100H" corresponds to a file register.
The cause of the error is that the file register file specified by the parameter cannot be created.
Check the amount of free space of the memory in which the file register file is created.
- Product Name
- MELSEC-L Series
- Series
- CPU