FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Maximum number of modules to be connected to L26CPU-(P)BT
FAQ
Maximum number of modules to be connected to L26CPU-(P)BT
What is the maximum number of modules connectable to L26CPU-(P)BT?
- Category :
Answer
Up to 40 modules.
When the branch module and extension module are used, use L26CPU-(P)BT CPU modules whose first 5 digits of the serial number are "13072" or later.
When the branch module and extension module are used, use L26CPU-(P)BT CPU modules whose first 5 digits of the serial number are "13072" or later.
- Product Name
- MELSEC-L Series
- Series
- L Series