FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Index modification when using extended data register in LCPU
FAQ
Index modification when using extended data register in LCPU
When I use internal user device (D) and extended data register (D) in LCPU, and specify an extended data register (D) area using index modification, an error with an error code 4101 occurs. What is the remedy?
Example)
- Internal user device: D0-8191
- Extended data register: D8192-315391
If Z0=10000 is specified when "D100Z0" is written, an error occurs.
Example)
- Internal user device: D0-8191
- Extended data register: D8192-315391
If Z0=10000 is specified when "D100Z0" is written, an error occurs.
- Category :
Answer
It is not possible to specify index modification to cross over the boundary between the internal user device (D) and the extended data register (D).
Change the internal user device (D) to 0 point and set all to the extended data register (D) allows index modification.
Change the internal user device (D) to 0 point and set all to the extended data register (D) allows index modification.
- Product Name
- MELSEC-L Series
- Series
- CPU