FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > How refresh devices for CC-Link remote inputs and outputs are assigned
FAQ
How refresh devices for CC-Link remote inputs and outputs are assigned
How are refresh devices for CC-Link remote inputs and outputs assigned?
- Category :
Answer
The refresh device setting of the CC-Link parameter assigns any devices to the I/O numbers greater than those assigned to the modules on the same base unit. The device set for the refresh device setting of RX/RY is assigned to the first address of station number 1 and the following devices of all other connected modules that are assigned to the successive addresses.
- Product Name
- Network Related Products
- Series
- CC-Link