FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > MODE switch setting for QJ61BT11N
FAQ
MODE switch setting for QJ61BT11N
What is the use of MODE switch for QJ61BT11N?
- Category :
Answer
The MODE switch can set the following modes.
- 0 to 4: Online mode
- 5 to 9: Line test mode
- A to E: Hardware test mode
Each mode in ascending order of set value provides communication speeds of 156Kbps, 625Kbps, 2.5Mbps, 5Mbps, and 10Mbps respectively.
- 0 to 4: Online mode
- 5 to 9: Line test mode
- A to E: Hardware test mode
Each mode in ascending order of set value provides communication speeds of 156Kbps, 625Kbps, 2.5Mbps, 5Mbps, and 10Mbps respectively.
- Product Name
- Network Related Products
- Series
- CC-Link