FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Links with a CC-Link local station cannot be made
FAQ
Links with a CC-Link local station cannot be made
Links with a CC-Link local station cannot be made. Are there any remedies?
- Category :
Answer
Check the following points.
(1) CC-Link cables have been properly connected.
(2) Station numbers and the transmission speed have been correctly set.
(3) The Network Parameter setting "Station Information Setting" of the master station has been correctly set.
(4) The Network Parameter setting "Operation Setting" of the local station has been correctly set (to the same number of
occupied stations as that set using "Station Information Setting" of the master station).
(5) Monitor the error code in link special registers SW0068 to SW006A of the master and local stations.
(1) CC-Link cables have been properly connected.
(2) Station numbers and the transmission speed have been correctly set.
(3) The Network Parameter setting "Station Information Setting" of the master station has been correctly set.
(4) The Network Parameter setting "Operation Setting" of the local station has been correctly set (to the same number of
occupied stations as that set using "Station Information Setting" of the master station).
(5) Monitor the error code in link special registers SW0068 to SW006A of the master and local stations.
- Product Name
- Network Related Products
- Series
- CC-Link