FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Whether or not multiple QJ72LP25-25 modules can be mounted
FAQ
Whether or not multiple QJ72LP25-25 modules can be mounted
Is it possible to mount two QJ72LP25-25 modules in a MELSECNET/H remote I/O station?
- Category :
Answer
No, only a single QJ72LP25-25 can be mounted (and is to be mounted on the CPU slot on a main base unit).
- Product Name
- Network Related Products
- Series
- MELSECNET/H