FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > 32-bit data assurance
FAQ
32-bit data assurance
What is the setting required to prevent 32-bit data from being separated in the CC-Link IE Controller Network?
- Category :
Answer
To assure 32-bit data, "Network Range Assignment" of the control station must satisfy the following conditions.
(1) The start device No. of LB is a multiple of 20H.
(2) The points assigned per station in LB is a multiple of 20H.
(3) The start device No. of LW is a multiple of 2.
(4) The points assigned per station in LW is a multiple of 2.
(1) The start device No. of LB is a multiple of 20H.
(2) The points assigned per station in LB is a multiple of 20H.
(3) The start device No. of LW is a multiple of 2.
(4) The points assigned per station in LW is a multiple of 2.
- Product Name
- Network Related Products
- Series
- CC-Link IE Controller Network