FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Parameter setting of CC-Link IE Field Network
FAQ
Parameter setting of CC-Link IE Field Network
Do I have to set the network range assignment parameters for all master station and slave stations?
- Category :
Answer
No, you do not have to set the network range assignment parameters for slave stations. By setting the network range assignment parameters for a master station, you can establish the connections with all slave stations.
- Product Name
- Network Related Products
- Series
- CC-Link IE Field Network