FAQ


FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Horizontal type robot > The tip of the robot is vibrating.
FAQ
The tip of the robot is vibrating.
The tip of the robot is vibrating.
Answer
Cause:
- The load conditions exceed the specified values(mass, inertia).
- The load condition settings are not suitable(HNDDAT and WRKDAT settings are not consistent with the load).
- The tip is being used near a singular point.
- Acceleration or deceleration is too sudden.
- The installation stand is not rigid enough.
- Vibrations from nearby equipment are being felt.
Measures:
- Check the load conditions and the parameter settings. Please also try to adjust the acceleration/deceleration time, the speed, and the teaching point where necessary.
- Check the condition of the unit's installation(including external vibrations).
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series