FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Vertical type robot > Breaker trips/overcurrent error occurs.
FAQ
Breaker trips/overcurrent error occurs.
Breaker trips/overcurrent error occurs
(cutting oil gets inside the robot body).
(cutting oil gets inside the robot body).
Answer
Cause:
- Deterioration in the packing.
- Scaling on the packing.
- Using a highly permeable cutting oil.
- An environment that exceeds the IP functionality.
Measures:
- In a mist environment, pull off and replace the packing every time the cover is removed.
- If a highly permeable cutting fluid is being used, or in an environment that exceeds the IP functionality, purge the air and take measures on the jacket.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series