FAQ


FAQAbout Products

- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Horizontal type robot > The T/B does not display anything.
FAQ
The T/B does not display anything.
The T/B does not display anything.
Answer
Cause:
- The fuse (4A fuse) installed at the bottom of the 24 V power supply circuit in the controller may have blown out.
For the fuse blowout, the emergency stop made by the customer may be the cause, or there may be a ground fault or short circuit with the 24 V power supply in the wiring of a door switch, enabling device, etc. - The T/B might be out of order.
Measures:
- Investigate and correct the ground fault or short circuit portion in the wiring made by the customer. Then, replace the fuse inside the controller.
- Product Name
- Industrial Robots MELFA
- Series
- F Series