FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
How can I set the current value of a thermal load relay?
Answer
A thermal load relay is set as full-load current of a motor. However, ifambient temperature is significantly different from 20℃ or the connectingwire is different from the standard wire size, it is necessary to correct theset value.
- Product Name
- Motor Starters
- Series
- MS-T/N