FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
How can I select a thermal load relay when it is installed in the deltaphase?
Answer
When installing a thermal load relay in the delta phase and detectingphase current, you select a heater designation that can be set to 1 / √ 3times of the motor full-load current value and you set the current value ofcurrent knob to 1 / √ 3 times of the motor full-load current value.
- Product Name
- Motor Starters
- Series
- MS-T/N