FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is the difference between main circuit 3-pole 2-element typeand 3-pole 3-element type of a solid state contactor?
Answer
The functions of 2 and 3 element type are almost same, but since theneutral pole (3/L2, 4/T2) of 3-pole 2-element type is connected inside, itis not possible to use in the delta phase to add the applicable capacity.Moreover, you need to install a disconnecting equipment at power supplyside and disconnect for maintenance all the time, since the load side isalways same potential as the power supply side.
- Product Name
- Motor Starters
- Series
- MS-T/N