Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23271
  • Release Date : 2018/09/12 15:11
  • Update : 2021/04/09 16:21
  • Print

About Low-voltage Power Distribution Products

Is there polarity in a control coil of SD-T* and SD-N*type?
Category : 

Answer

SD-T12 to T32 and SD-N600, N800 type operation coil terminals have polarity.
Connect terminal mumber A1 (+) to the positive and A2 (-) to the negative sides.
Product Name
Motor Starters
Series
MS-T/N
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?