FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
According to the catalog, the coil designation of S-T and S-N type isAC200V and SD-T, and the coil designation of SD-N is DC100V, buthow about other coil designation?
Answer
For other coil designation, it can be calculated as below.1. For S-T* and S-N* type (AC operation type)(1) Input (Instantaneous, constant) power consumption : This value isalmost same as the value described in our catalog.(2) Operating voltage : It is approximate voltage proportion. (When it isAC100V coil, (100/200)* the value described in our catalog)(3) Coil current : Approximately input (instantaneous, constant) / appliedvoltage2. For SD-T* and SD-N* type (DC operation type)(1) Power consumption : This value is almost same as the value describedin our catalog.(2) Operating voltage : It is approximate voltage proportion. (When it isDC24V coil, (24/100)* the value described in our catalog)(3) Coil current : Approximately power consumption / coil voltage(4) Time constant of coil : This value is almost same as the valuedescribed in our catalog.
- Product Name
- Motor Starters
- Series
- MS-T/N