Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23278
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is the voltage range which can be applied to a control coil of S-T,S-N,SD-T and SD-N type?
Category : 

Answer

At ambient temperature 40℃, the rated voltage (frequency) is applied to acontrol coil, and after temperature rise and saturation, it can operatewithout any trouble at 85 to 110% of the coil rated voltage. Whenapplying the voltage continuously, please use at 95 ~ 100% of that.
Product Name
Motor Starters
Series
MS-T/N
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?