FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is voltage range that can be applied to a control coil of SR-T*and SRD-T* type?
Answer
At ambient temperature 40℃, the rated voltage (frequency) is applied tothe control coil, and after temperature rise and saturation, it can operatewithout any trouble at 85 to 110% of the coil rated voltage. Whenapplying the voltage continuously, please use at 95 ~ 100% of that.
- Product Name
- Motor Starters
- Series
- MS-T/N