FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is the minimum applicale voltage and current at auxiliarycontact of SD-Q* type?
Answer
The minimum applicable load voltage and current are as follows. Contactreliability is indicated by fault rate λ60 (Number of faults / Operatingcycles per one contact) at the reliability level 60%.1. Main contact: 24V300mA (Contact reliability 1*10-7/ time)2. Auxiliary contact: 5V3mA (Contact reliability 5*10-7/ time)
- Product Name
- Motor Starters
- Series
- MS-T/N