FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is withstand voltage of S-T* and S-N* type?
Answer
In the withstand voltage test, 2500V is applied for 1 min. The appliedlocation is as follows.1. Between the conductive part and the grounded metal part, and theconductive part and the control circuit (grounded) with the contact closed2. Between each pole with the contact closed3. Between the conductive part and the grounded metal part and thecontrol circuit (grounded) with the contact opened4. Between the power supply side terminal and the load side terminal withthe contact opened5. Between the conductive part of the control circuit and the groundedmetal part6. Between one of the control circuit and other circuits (grounded)
- Product Name
- Motor Starters
- Series
- MS-T/N