FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is the minimum applicable voltage and current of S-T*, SD-T*,SL-T*, SLD-T*, S-N*, SD-N*, SL-N* and SLD-N* type?
Answer
The minimum applicable load is as follows. Contact reliability is indicatedby fault rate λ60 (Number of fault / Operating cycles per one contact) atthe reliability level 60%.1. Main contact: 48V200mA (Contact reliability 1*10-7/ time)2. Auxiliary contact: 20V3mA (Contact reliability 1*10-7/ time)
- Product Name
- Motor Starters
- Series
- MS-T/N