Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23424
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:39
  • Print

Compatibility of communication units for the GOT1000 series

Answer

For the GOT2000 series, the following communication units for the GOT1000 series can be used.
■ GT27, GT25 (excluding GT2505, GT2510-WX, and GT2507-W)
・ GT15-QBUS, GT15-QBUS2,
 GT15-ABUS, GT15-ABUS2,
 GT15-75QBUSL, GT15-75QBUS2L,
 GT15-75ABUSL, GT15-75ABUS2L,
 GT15-RS2-9P, GT15-RS4-9S, GT15-RS4-TE,
 GT15-J71LP23-25, GT15-J71BR13,
 GT15-J71GP23-SX,
 GT15-J71GF13-T2,
 GT15-J61BT13,
 GT01-RS4-M

■ GT2505
・ GT01-RS4-M, GT10-9PT5S, GT14-RS2T4-9P

■ GT2510-WX, GT2507-W,
 GT2104-R, GT2104-PMBD, GT2104-PMBDS,
 GT2103-PMBD, GT2103-PMBDS
・ GT01-RS4-M

■ GT2105
・ GT01-RS4-M, GT10-9PT5S

The following communication units for the GOT1000 series cannot be used.

1. GT15-J71E71-100
 Please replace it with the standard interface (Ethernet) of the GOT, or use the communication unit (GT25-J71E71-100) dedicated to the GOT2000 series.

2. GT15-RS2T4-9P, GT15-RS2T4-25P
 Use the standard interface (RS422/485) of the GOT.
* For GT15-RS2T4-25P, a commercially available conversion connector for converting 25-pin D-sub to 9-pin D-sub is required separately.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Communication unit
Series
GOT2000 Series

May I have your opinion?

Inquiries