FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Compatibility of communication units for the GOT1000 series
FAQ
Compatibility of communication units for the GOT1000 series
Can communication units for the GOT1000 series be used for the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
For the GOT2000 series, the following communication units for the GOT1000 series can be used.
■ GT27, GT25 (excluding GT2505, GT2510-WX, and GT2507-W)
・ GT15-QBUS, GT15-QBUS2,
GT15-ABUS, GT15-ABUS2,
GT15-75QBUSL, GT15-75QBUS2L,
GT15-75ABUSL, GT15-75ABUS2L,
GT15-RS2-9P, GT15-RS4-9S, GT15-RS4-TE,
GT15-J71LP23-25, GT15-J71BR13,
GT15-J71GP23-SX,
GT15-J71GF13-T2,
GT15-J61BT13,
GT01-RS4-M
■ GT2505
・ GT01-RS4-M, GT10-9PT5S, GT14-RS2T4-9P
■ GT2510-WX, GT2507-W,
GT2104-R, GT2104-PMBD, GT2104-PMBDS,
GT2103-PMBD, GT2103-PMBDS
・ GT01-RS4-M
■ GT2105
・ GT01-RS4-M, GT10-9PT5S
The following communication units for the GOT1000 series cannot be used.
1. GT15-J71E71-100
Please replace it with the standard interface (Ethernet) of the GOT, or use the communication unit (GT25-J71E71-100) dedicated to the GOT2000 series.
2. GT15-RS2T4-9P, GT15-RS2T4-25P
Use the standard interface (RS422/485) of the GOT.
* For GT15-RS2T4-25P, a commercially available conversion connector for converting 25-pin D-sub to 9-pin D-sub is required separately.
■ GT27, GT25 (excluding GT2505, GT2510-WX, and GT2507-W)
・ GT15-QBUS, GT15-QBUS2,
GT15-ABUS, GT15-ABUS2,
GT15-75QBUSL, GT15-75QBUS2L,
GT15-75ABUSL, GT15-75ABUS2L,
GT15-RS2-9P, GT15-RS4-9S, GT15-RS4-TE,
GT15-J71LP23-25, GT15-J71BR13,
GT15-J71GP23-SX,
GT15-J71GF13-T2,
GT15-J61BT13,
GT01-RS4-M
■ GT2505
・ GT01-RS4-M, GT10-9PT5S, GT14-RS2T4-9P
■ GT2510-WX, GT2507-W,
GT2104-R, GT2104-PMBD, GT2104-PMBDS,
GT2103-PMBD, GT2103-PMBDS
・ GT01-RS4-M
■ GT2105
・ GT01-RS4-M, GT10-9PT5S
The following communication units for the GOT1000 series cannot be used.
1. GT15-J71E71-100
Please replace it with the standard interface (Ethernet) of the GOT, or use the communication unit (GT25-J71E71-100) dedicated to the GOT2000 series.
2. GT15-RS2T4-9P, GT15-RS2T4-25P
Use the standard interface (RS422/485) of the GOT.
* For GT15-RS2T4-25P, a commercially available conversion connector for converting 25-pin D-sub to 9-pin D-sub is required separately.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit
- Series
- GOT2000 Series