Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23429
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:44
  • Print

Screen gesture function when the remote personal computer operation function is used

Can the screen gesture function on the remote personal computer operation screen when the remote personal computer operation function is used?
Category : 

Answer

The screen gesture function cannot be used on the remote personal computer operation screen when the remote personal computer operation function is used. The following are the reasons.

1. For the remote personal computer operation function (Serial)
 The operation position information is not communicated to the personal computer correctly, and thus a malfunction occurs.

2. For the remote personal computer operation function (Ethernet)
 The remote personal computer operation screen is displayed as an overlap window. However, the overlap window is hidden in the screen gesture mode.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (remote personal computer operation)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries