FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21 > Ethernet connection between multiple GOTs and the QnUDVCPU
FAQ
Ethernet connection between multiple GOTs and the QnUDVCPU
I want to connect multiple GOT2000 series models and one QnUDVCPU by Ethernet by using the Ethernet port built in the CPU.
How can I set it?
How can I set it?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The following describes an example of settings to connect multiple GT27, GT25, or GT21 models (Ethernet connection models) and the Ethernet port built in the QnUDVCPU by Ethernet.
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDEH
IP address 192.168.3.39
Port No. 5006
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
(4) Set a different station number and GOT IP address for (1) to (3) above for each GOT.
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection (Set this item for each GOT.)
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDEH
IP address 192.168.3.39
Port No. 5006
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
(4) Set a different station number and GOT IP address for (1) to (3) above for each GOT.
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection (Set this item for each GOT.)
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series